QT5 camera, no service found for - "org.qt-project.qt.camera"
Hi team,
I have an STM32MP157 board with the following git branch.
a. buildroot: remotes/origin/st/2023.02.6
b. buildroot-external-st: remotes/origin/st/2023.02.2
I got the error message "no service found for - "org.qt-project.qt.camera"" when I run the QT5 example camera code.
but "mediaservice" is in /usr/lib/qt/plugins/.
The following are plugins:
# ls /usr/lib/qt/plugins/
audio imageformats qmltooling
bearer mediaservice scenegraph
egldeviceintegrations platforms video
generic playlistformats
export QT_DEBUG_PLUGINS=0 //open debug
export QT_PLUGIN_PATH=/usr/lib/qt/plugins/
root@buildroot:/usr/lib/qt/examples/multimediawidgets/camera
# ./camera
defaultServiceProvider::requestService(): no service found for - "org.qt-project.qt.camera"
The libraries appear to be loaded.
# ldd ./camera
linux-vdso.so.1 (0xbed92000)
libatomic.so.1 => /lib/libatomic.so.1 (0xb6f20000)
libQt5MultimediaWidgets.so.5 => /usr/lib/libQt5MultimediaWidgets.so.5 (0xb6ee0000)
libQt5Multimedia.so.5 => /usr/lib/libQt5Multimedia.so.5 (0xb6e10000)
libQt5Widgets.so.5 => /usr/lib/libQt5Widgets.so.5 (0xb6950000)
libQt5Gui.so.5 => /usr/lib/libQt5Gui.so.5 (0xb6590000)
libQt5Network.so.5 => /usr/lib/libQt5Network.so.5 (0xb6450000)
libQt5Core.so.5 => /usr/lib/libQt5Core.so.5 (0xb5fc0000)
libGLESv2.so.2 => /usr/lib/libGLESv2.so.2 (0xb5d9b000)
libstdc++.so.6 => /usr/lib/libstdc++.so.6 (0xb5c20000)
libm.so.6 => /lib/libm.so.6 (0xb5bc0000)
libgcc_s.so.1 => /lib/libgcc_s.so.1 (0xb5b80000)
libc.so.6 => /lib/libc.so.6 (0xb5a20000)
/lib/ld-linux-armhf.so.3 (0xb6f84000)
libQt5OpenGL.so.5 => /usr/lib/libQt5OpenGL.so.5 (0xb59c0000)
libpng16.so.16 => /usr/lib/libpng16.so.16 (0xb5970000)
libz.so.1 => /usr/lib/libz.so.1 (0xb5930000)
libpcre2-16.so.0 => /usr/lib/libpcre2-16.so.0 (0xb58c0000)
libgthread-2.0.so.0 => /usr/lib/libgthread-2.0.so.0 (0xb5890000)
libglib-2.0.so.0 => /usr/lib/libglib-2.0.so.0 (0xb5760000)
libGAL.so => /usr/lib/libGAL.so (0xb5697000)
libVSC.so => /usr/lib/libVSC.so (0xb5388000)
libpcre.so.1 => /usr/lib/libpcre.so.1 (0xb5330000)
libpthread.so.0 => /lib/libpthread.so.0 (0xb5300000)
librt.so.1 => /lib/librt.so.1 (0xb52d0000)
Would you give an advise?
Thanks for reading.