Skip to main content
Visitor II
November 24, 2021
Question

Questions about burning erroI found the following errors when I burned kernel alone and starterpackage. May I ask why this was caused? The kernel is through https://github.com/STMicroelectronics/meta-st-stm32mp/blob/dunfell/recipes-kernel/linux/linux

  • November 24, 2021
  • 5 replies
  • 6474 views

I found the following errors when I burned kernel alone and starterpackage. May I ask why this was caused? The kernel is through https://github.com/STMicroelectronics/meta-st-stm32mp/blob/dunfell/recipes-kernel/linux/linux-stm32mp/README.HO W_to.txt teaching burn, Starterpackage is delivered via STM32_Programmer_CLI -c port= USb1 -w Flashlayout_st - image - weston/trusted/FlashLayout_sdcard_stm32mp157c - dk2 - trusted. TSV

    This topic has been closed for replies.

    5 replies

    Graduate II
    November 24, 2021

    Please avoid putting the entire question in the Summary field, and that posted like are valid.

    Complaining that generated image lacks a partition tables, so perhaps missing a step/stage of process, or not picking final file, but rather an intermediate one.​

    Ffu.1Author
    Visitor II
    November 25, 2021
    I downloaded en. Flash-stm32mp1-openstlinux-5.10-dunfall-mp1-21-03-31.tar_v3.0.0.xz and burned its firmware. I don't know what middleware you mean. I re-uploaded flashlayout_sdcard_stm32mp157C-dk2-trusted. TSV and download log for you to see.
    Technical Moderator
    November 24, 2021

    Hi @Ffu.1​ ,

    You flashlayout log looks a bit strange .. is it complete ?

    Did you customized content of FlashLayout_sdcard_stm32mp157c-dk2 -trusted.TSV ?

    Please clarify what you mean by "I burned kernel alone and starterpackage"

    Olivier

    Ffu.1Author
    Visitor II
    November 25, 2021
    Dear Olivier:
    Thank you help. Your reply to your question is as follows: ① I have re-sent you a complete flashout log as shown below; Flashlayout_sdcard_stm32mp157c-dk2-trusted.TSV I downloaded en. Flash-stm32mp1-openstlinux-5.10-dunfell-mp1-21-03-31.tar_v3.0.0.xz and burned its firmware. ③ I mean the following file error is caused by different SDK, one is in en.flash-stm32mp1-OpenStLinux-5.10-Dunfell-mp1-21-03-31.tar_v3.0.0. xz, which is the starter Package. Another error occurs when the kernel package compiled in developer-packageper is burned
    Technical Moderator
    November 25, 2021

    Hi @Ffu.1​ ,

    Can you provide me exact reference of your DK board.

    May you have another board available for a try ?

    Thanks,

    Olivier

    Ffu.1Author
    Visitor II
    November 25, 2021

    I find that sometimes it can be successfully burned and sometimes it is not successful. I don't know if it is the board problem. I don't know if you want to

    Technical Moderator
    November 25, 2021

    Hi @Ffu.1​ ,

    What is your SDcard reference also ? Can you try another one ?

    Seems you flash from Linux station ? Which OS ?

    Thanks

    Olivier