Questions about setting the ADC clock on the M4 core side
Hi ST
I have a question when setting the ADC Clock on the M4 Core side.
The STM32MP151C datasheet states that the ADC Clock can be set up to 36Mhz.
When the AHB clock is 200Mhz, what clock will it work with if I set "ADC ClockPrescaler" to "ADC_CLOCK_SYNC_PCLK_DIV4"?
When calculated, ADC Clock is 50Mhz.
However, the maximum operating clock in the datasheet is 36Mhz.
Which ADC clock will it work with?
I would be grateful if you could tell me the answer.
Regards
Machilus