Skip to main content
Visitor II
February 25, 2021
Question

Questions about STM32MP157C-DK2

  • February 25, 2021
  • 1 reply
  • 984 views

Hello! I have just discovered that kit I would like to use to develop a new testing system within the company where I am working. However, I have some questions about it:

  • What kind of additional card could we use to apply 24V to the board's input (I have to use the output signal of the inductive sensor currently used)?
  • Does it exist a card which can directly get 24V as an input voltage (or is it always 5V or 3.3V)?
  • How many analogical, numerical and On/Off I/O does the kit's board have?
  • Could we use some software like Matlab to analyse the output signals of that card?

I truly thank you in advance for your answers!

Sincerely,

    This topic has been closed for replies.

    1 reply

    ST Employee
    March 9, 2021

    Hello @NAnt.3

    In case you haven’t seen yet, some information can be found in the User Manual for the board on st.com

    https://www.st.com/resource/en/user_manual/dm00591354-discovery-kits-with-stm32mp157-mpus-stmicroelectronics.pdf

    -         Input voltage is only 5 V / 3 A USB Type-C™power supply input

    -         Available IO’s can be seen in the

    ◦ GPIO expansion connector (Raspberry Pi® shields capability)

    ◦ Arduino™ Uno V3 expansion connectors

    Best Regards

    JM