Questions about TrustZone Configuration on STM32MP135F-DK
Hello,
I am currently engaged in a project that involves using TrustZone to securely display an image on the STM32MP135F-DK. I'm facing several challenges, especially in configuring the framebuffer for secure display purposes:
1. Running the 'hello_world' Example: I am experiencing issues with running the TrustZone 'hello_world' example from OP-TEE on the board. I tried to get the OP-TEE version that supports STM32MP1, compile OP-TEE, and copy the output OP-TEE trustzone's hello_world binary to the board. But it cannot be directly executed on the board.
2. Triggering TrustZone: After installing the SDK for STM32MP135F-DK and recompiling the kernel and drivers as per the instructions from the wiki, I am unsure of how to proceed with testing the OP-TEE 'helloworld' example. Should I compile it within the SDK and then transfer the binary to the board?
3. Secure Framebuffer Configuration: I noticed that the dts file for STM32MP135F-DK already defines a secure framebuffer. Does it provide interfaces to write to the framebuffer, or should I consider writing a driver myself?
I would greatly appreciate any advice you could provide on these issues. Thank you for your time!