RGB display with dead zone
Hello all,
I currently have to deal with a display which has an inactive zone in the middle. Its "interface" resolution is 540x1280px, but the 140px columns in the middle are not connected to the screen. That is, the display is of 400x1280px of resolution but the whole 540 columns have to be provided through its interface. In order to display a 400x1280px image, I need to split it into two 200x1280px regions and send them with the dead zone in the middle.
Here is a diagram about how this is working (active are in red):

I wonder if there is a way to use the LTDC peripheral to do this in an efficient way. I am thinking about using layers and/or windows to achieve this. Currently I am using QT to generate the content on-screen.
Does anybody have a clue on how to deal with this kind of component?
Thank you very much in advance!