Skip to main content
Visitor II
September 3, 2021
Solved

RPMSG SDB0 Driver Issue

  • September 3, 2021
  • 2 replies
  • 1559 views

Hi all,

I am trying to achieve DDR data transfer between M4 and A7.

So I followed How to exchange data buffers with the coprocessor - stm32mpu article and built a yocto image.

I have stripped down the logic analyzer application : here .

  1. On CM4 side it just transfers data from a another MCU pushing in data at UART7 and transferring that via DMA to DDR buffer.
  2. SDB Driver unchanged.
  3. On the Application side , I have removed all GTK related things and just stripped it down to receive data to DDR buffer and print to a console.

I have few questions of concerns:

In case of the CM4 code provided here : Link

There no support in the latest cube-mx to create an RPMSG_HDR_HandleTypeDef type object which might be labelled as /dev/tpmsg-sdb type in user space application.

Although the data structure is similar to VIRT_UART_HandleTypeDef. So I went ahead and made and rpmsg-sdb object of the later type.

Now when I run my stripped down application part of attached zip. I get below error on A7-console :

CA7 : Forward efd info for buf0 with mFdSdbRpmsg:5 and efd:6
./backend: failed to set efd: Inappropriate ioctl for device

Note that now I get 3 devices : ttyRPMSG0 , 1 , 2. So in order to identify which is the sdb one I initialized it at the last in M4 code. Not sure if that is right way.

Kindly advice what might be potential root cause of issue here.

    This topic has been closed for replies.
    Best answer by NPal.2

    Update : Never mind. Solved it. There was a minor change in the CM4 project, where in there was an extra file set : rpmsg_hdr.c / .h was created to handle the data transfer over rpmsg-sdb channel. After making those changes in the CM4 side. Seems to work now perfectly.

    2 replies

    NPal.2Author
    Visitor II
    September 3, 2021

    Update : Looks like the stm32_rpmsg_sdb driver gets loaded , but there is no device called : /dev/rpmsg-sdb which shows up.

    NPal.2AuthorAnswer
    Visitor II
    September 3, 2021

    Update : Never mind. Solved it. There was a minor change in the CM4 project, where in there was an extra file set : rpmsg_hdr.c / .h was created to handle the data transfer over rpmsg-sdb channel. After making those changes in the CM4 side. Seems to work now perfectly.