Running a STM32MP157A-DK1 in 85 d°C, makes it crash.
I'm testing a stm32mp157a-dk1 in 85 °C for a project.
The setup is basic, power from usb and network over ethernet to a control computer outside the chamber. I ssh in to the board to check that its alive and put some load on the cpu.
Even without load. the board seems to crash, I lose the SSH connection and a led blinking blue goes dark, LD 7/8 I think.
The STM32MP157-A should be rated for those conditions right ? could it be some peripheral chip on the board that causes the crash?
Cheers