S24_LE support on I2S of STM32MP1 line
Hi,
what's the state of the S24_LE format support on the STM32MP1 line of boards? It seems that S16_LE and S32_LE formats are supported on the I2S dai, however S24_LE is rather unavailable. Is there a way to somehow enable it (maybe through Cube MX) or is it completely unsupported?
When running alsa speaker-test utility with hardware devices (not default) the S24_LE format is being rejected.
Thanks!