Secure boot TF-A error - BL2: Failed to load image id 1 (-80) : STM32MP2
Hi,
I am trying to boot a signed TF-A image on my STM32m257f compiled with TRUSTED_BOARD_BOOT support (Compiled in f-a-stm32mp.inc recipe from meta-st-stm32mp, mickledore branche).
When the board is powered up, i got this error:
NOTICE: CPU: STM32MP257FAI Rev.B
NOTICE: Model: STMicroelectronics STM32MP257F-EV1 Evaluation Board
NOTICE: Board: MB1936 Var1.0 Rev.C-01
NOTICE: BL2: v2.8-stm32mp2-r2.0(release):lts-v2.8.15-dirty(567af710)
NOTICE: BL2: Built : 00:51:33, Jan 26 2024
NOTICE: TRUSTED_BOARD_BOOT support enabled
ERROR: BL2: Failed to load image id 1 (-80)
I've already fuse my PKHTH with the stm32key command and my binary is signed with the right key. The board boots normally when I install a TF-A binary without TRUSTED_BOARD_BOOT support.
Do you have any idea please?
Thanks