Skip to main content
Graduate II
June 2, 2024
Solved

Should I use length matching on all differential pairs?

  • June 2, 2024
  • 1 reply
  • 2967 views

Even if I route the differential pairs, one pair will always be longer than the other.

Should I route an extra path, like a sawtooth or tromebone on the shortest pair to make booth differential pair equal in length?

I see that the STM32MP1 dev-kit does not use this, either on DDR or Gigabit Ethernet, but I have heard that it's recommended to make sure that all differential pairs have the same length.

HDMI:

HDMIHDMI

 

Gigabit Ethernet:

Gigabit EthernetGigabit Ethernet

USB OTG: 

USB OTG 1USB OTG 1

 

USB OTG:

USB OTG 2USB OTG 2

DQS1:

DQS1DQS1

DQS0:

DQS0DQS0

DDR CLK:

DDR_CLKDDR_CLK

    This topic has been closed for replies.
    Best answer by PatrickF

    Hi, it is vice versa, the USB_DM should be longer than USB_DM by 507um.

    The AN lists the package inner length differences (i.e. negative value mean DM is shorter than DP by 507um inside the package)

    Sound logical to have a value around 500um if you look at ball locations Vs the package edge where you are going to escape the tracks).

    PatrickF_1-1717481736916.png

    Regards.

     

     

     

    1 reply

    Technical Moderator
    June 3, 2024

    Hi @DMårt 

    for DDR, the lenghts requirements are provided in AN5122 and could be checked with associated excel sheets.

    Usually, seems experts give slightly higher priority to good differential routing rather than strict length matching.

     

    e.g. for DSI in STM32MP15, we provided in AN5031 this guidelines as rule of thumb. +/-5mils is somewhat hard to achieve (note that we already have partial compensation for length difference between two balls when they are diagonal or stacked).

    PatrickF_0-1717402165031.png

     

    For other interfaces (Ethernet, USB, HDMI, etc...), you have to refer to the related standard requirements or associated components routing guidelines.

     

    Regards

    DMårtAuthor
    Graduate II
    June 3, 2024

    Hi @PatrickF 

     

    The difference between the CLK_P and CLK_N was about 1 mm.

     

    Yes. I found that the pad for the USB has a pitch of 507 um. That means I should make the N-track 507 um shorter than P-track due to internal length of N-track?

     

     

    PatrickFAnswer
    Technical Moderator
    June 4, 2024

    Hi, it is vice versa, the USB_DM should be longer than USB_DM by 507um.

    The AN lists the package inner length differences (i.e. negative value mean DM is shorter than DP by 507um inside the package)

    Sound logical to have a value around 500um if you look at ball locations Vs the package edge where you are going to escape the tracks).

    PatrickF_1-1717481736916.png

    Regards.