ST-HSMv2 programming - personalization data & fw id
Hi,
I want to perform the SSP process as detailed at:
(I also went over the STM32_prog documents)
I am now trying to program my HSMv2 card and I don't understand which file I need to provide in "Personalization data file"
(Trusted Package Creator - HSM Tab)
There are 2 options:
- STM32MP1_5000200A_SSP_01000000_00000000.enc.bin
- STM32MP1_5000300A_SSP_01000000_00000000.enc.bin
I don't understand which one I need to pick
my MPU is "STM32MP157CAB3" (Rev Z)
is it 5000300 because of the "3" after the "CAB" ?
The "5000" part I understand, I can see this value in the DFU device info
The "200" vs "300" I don't understand
According to the Docs, I need to know the product ID of my MPU
And they suggest using "STM32_Programmer_CLI –c port=swd –gc "certificate.bin"" to find out this value
but this command is failing:
"an error occurred while uploading data from the virtual partition 0xF1"
Another thing I don't quite fully understand is the value of "Firmware identifier" field in the HSM tab
Is it any string I want ?
The example images show "SSP_MPU"
Thanks,
Michael