Starting M4 from BootRom
Is there a way to directly start M4 and run M4 firmware from BootRom.
I am aware of the Engineering mode, however it requires the help of a debugger to copy the M4 firmware into the memory and run it. I like to do the same but in stand alone mode.
I am also aware that M4 can be started and run M4 firmware using SSBL, however we want the M4 firmware to configure clocks instead SSBL. Some could point out why not then use a M4 based microcontroller instead of the MPU, but we have a specific requirement to boot from BootRom to M4 on the MPU.
I am thinking about an idea to store M4 firmware as FSBL with the correct headers on one of the Flash devices (NOR/NAND Flash), once FSBL is stated by bootRom, copy M4 firmware and run it.
I have not come across such approach, that is why I like to ask if this is going to be even possible?