STLINK-V3PWR quality control
Hello,
The QC for STLINK-V3PWR assembled in France seems to be very bad. I received a unit that doesn't work out of the box (when USB is connected the status leds stay off, AUX power outputs 3.3V, host computer doesn't detect V3PWR).
The same host computer works just fine with another V3PWR unit.
I decided to check the faulty unit out to see if there is a trivial fix for the issue (since the return shipping to the distributor is quite expensive). I found out that the USB3340 constantly has RESETB signal low, since it also has VCCIO applied this means that it is effectively disabled and tristated. Trying to trace where RESETB goes, I found U35 on the other side partially lifted, underneath U35 there was a small SMD resistor propping it up. I don't know how this could have passed QC.
Reworking U35 unfortunately did not improve anything. Unfortunately there are not schematics available for the V3PWR to make such troubleshooting easier. U35 seems to be a dual op-amp....
Is there any chance to get the schematics of STLINK-V3PWR? Or at least information what controls the RESETB signal on the V3PWR's USB PHY?
Thanks!