Skip to main content
Technical Moderator
March 3, 2020
Question

STM32 MPUs NEW Ecosystem Release V1.2

  • March 3, 2020
  • 3 replies
  • 1537 views

Dear STM32 MPU Community,

We are please to announce that New MP1 Ecosystem V1.2.0 ! is available since the 25th of February 2020.

This is version of each component of this release and features to be highlighted ( most expected in this community ) :

Openstlinux-20-02-19 :

  • Added support for STM32MP15x Rev.Z fixing a bug preventing to boot from some eMMC parts.
  • Added support for new 800 MHz part numbers (D and F) 
  • Configured access to pre-build package repository with "apt-get"

see https://wiki.st.com/stm32mpu/wiki/Package_repository_for_OpenSTLinux_distribution

STM32CubeMP1-v1.2.0 :

  • Added Keil® Project examples on STM32MP157C-DK2
  • Added IAR™ Project examples on STM32MP157C-DK2
  • Added CubeIDE Project examples on STM32MP157C-DK2
  • Added new FreeRTOS + OpenAMP example

STM32CubeProgrammer-v2.4.0 :

  • Flashload speed improvement over USB on Windows PC
  • Parallel programming on several targets

STM32CubeMX-v5.6 :

  • DDR
    • Added support for LPDDR on 18x18, 16x16 packages
    • DDR tuning parameters saving: see the restriction below in this article
  • Added support for Engineering mode
  • Added tutorial Videos
    • DDR tuning [1]
    • How to customize a DT from an ST board [2]

STM32CubeIDE V1.3.0 :

  • some bug fix and enhancement for a better user experience

Refer to https://wiki.st.com/stm32mpu/index.php/STM32MP15_ecosystem_release_note

for complete description and download.

 Major Update on Wiki Documentation !

As usual, Ecosystem release has been opportunity to update and enrich the Wiki Online User Document ! 

Please visit https://wiki.st.com/stm32mpu/wiki/Main_Page

Hope you will enjoy this new release.

Looking forward to read you on this Community !

    This topic has been closed for replies.

    3 replies

    Visitor II
    March 14, 2020

    Hi,

    Can I install python package using ecosystem-release-v12 on STM32MP1DK2? Is X-LINUX-AI-CV OpenSTLinux expansion package is compatible with this release?

    I am looking for python package response, json etc. In Linux, we can install package using pip install "package name". Is this also possible with this latest release?

    If not then can you please share other alternatives?

    Thanking you,

    Saurabh

    Visitor II
    March 16, 2020

    Sorry I resolved the above problem. Please ignore it.

    Visitor II
    July 21, 2020

    How did you solved the problem? Can you please elaborate ? I also need to have git and python installed.