STM32MP1 - Bare metal on A7
Hi,
I have a current project using the M7 that I need to port over to the A7. The goal is to be running bare-metal code on the A7, like we are on the M7.
Currently, I am following this open source guide to run bare-metal on the A7 and it seems to work fine.
Does ST provide any support for running bare-metal on the A7? Does the stmCubeIDE allow for this? Is there a guide on porting a project from the M7 over to the A7?
Any help or information regarding this would be helpful!
Thanks!