STM32MP1 DSI voltage level
I would like to clear up some confusion regarding the DSI VIO, the stm32mp157a datasheet mentions "1.2 V I/O for DSI interface" but in the EV1 kit the LCD used (the RK055AHD042-CT, for which it's impossible to find a datasheet for, could that be shared too?) uses the RM68200 driver which seems to require 1.8V for IO.
The LCD I would like to use also requires 1.8V so I'm wondering if I need a high-speed voltage translator or will the STM32MP1 support my LCD?