STM32MP1 ECO Unused GPIO busy after gpioset
Kernel tree does not assign any driver to pin PZ2. After gpioset -c gpiochip11 2=1, the pins goes actually high (from low) but the gpioset program stalls. SSH at that moment into the device shows:
line 0: "PZ0" input
line 1: "PZ1" input
line 2: "PZ2" output consumer="gpioset"
line 3: "PZ3" input
line 4: "PZ4" input consumer="kernel"
line 5: "PZ5" input consumer="kernel"
line 6: "PZ6" input
line 7: "PZ7" input
Aborting CTRL-C/Z gpioset causes the device to be busy upon a next set.
Is there a way to set the pin and the client release itself as consumer of GPIO pin to be able to change the pin later back to low?
root@stm32mp1:~# gpioset -c gpiochip11 2=1
^Z[1]+ Stopped gpioset -c gpiochip11 2=1
root@stm32mp1:~# gpioset -c gpiochip11 2=0
gpioset: unable to request lines on chip '/dev/gpiochip11': Device or resource busy
root@stm32mp1:~# gpioget -c gpiochip11 2
gpioget: unable to request lines: Device or resource busy