STM32MP1 ecosystem 3.10 Developer package kernel fails to build on Ubuntu 21.10 (glibc 3.22 not found)
make ARCH=arm uImage vmlinux dtbs LOADADDR=0xC2000040
GEN Makefile
HOSTCC scripts/mod/mk_elfconfig
/media/user/H3D1P2/Tools/STM32MP1/STM_ECO_3.10/Developer-Package/SDK/sysroots/x86_64-ostl_sdk-linux/usr/bin/ld: /usr/lib/gcc/x86_64-linux-gnu/11/liblto_plugin.so: error loading plugin: /media/user/H3D1P2/Tools/STM32MP1/STM_ECO_3.10/Developer-Package/SDK/sysroots/x86_64-ostl_sdk-linux/lib/libc.so.6: version `GLIBC_2.33' not found (required by /usr/lib/gcc/x86_64-linux-gnu/11/liblto_plugin.so)
collect2: error: ld returned 1 exit status
make[2]: *** [scripts/Makefile.host:95: scripts/mod/mk_elfconfig] Error 1
make[1]: *** [/media/user/H3D1P2/Tools/STM32MP1/STM_ECO_3.10/Developer-Package/stm32mp1-openstlinux-5.10-dunfell-mp1-21-11-17/sources/arm-ostl-linux-gnueabi/linux-stm32mp-5.10.61-stm32mp-r2-r0/linux-5.10.61/Makefile:1214: prepare0] Error 2
make: *** [/media/user/H3D1P2/Tools/STM32MP1/STM_ECO_3.10/Developer-Package/stm32mp1-openstlinux-5.10-dunfell-mp1-21-11-17/sources/arm-ostl-linux-gnueabi/linux-stm32mp-5.10.61-stm32mp-r2-r0/linux-5.10.61/Makefile:185: __sub-make] Error 2
sudo apt-get install libc6
Reading package lists... Done
Building dependency tree... Done
Reading state information... Done
libc6 is already the newest version (2.34-0ubuntu3).
0 upgraded, 0 newly installed, 0 to remove and 0 not upgrad
Linux H3U1 5.13.0-28-lowlatency #31-Ubuntu SMP PREEMPT Thu Jan 13 18:29:33 UTC 2022 x86_64 x86_64 x86_64 GNU/Linux