Skip to main content
Visitor II
June 24, 2022
Solved

STM32MP1 public key hash (OTP WORD 24 to 31)

  • June 24, 2022
  • 4 replies
  • 1491 views
  1. Is it possible to use OTP WORD 24 to 31 without enable security boot with STM32MP1 part numbers which didn't has security boot option like STM32MP157A/D?
  2. Same as above but with STM32MP1 part numbers which has security boot option like STM32MP157C/F?
    This topic has been closed for replies.
    Best answer by PatrickF

    Hi @mikefae​ 

    See note 3 of Table 17 in RM0436 Rev.6

    In addition to Reference Manuel, the datasheet ordering information will tell you which device has secure-boot option (here STM32MP15xD or F could fit your needs).

    Regards,

    4 replies

    Technical Moderator
    June 27, 2022

    Hi mikefae (Community Member)

    As long as authentication is not used, it is possible to use OTP 24-31 for other purposes.

    Regards,

    Olivier

    Technical Moderator
    June 27, 2022

    Just one precision on STM32MP157A/D parts, OTP24-31 are permanently write locked on devices without secure-boot option as specified in the Reference Manual. So the above it is only possible on C/F parts.

    Regards,

    Olivier

    mikefaeAuthor
    Visitor II
    June 27, 2022

    Hello Olivier,

    Thank you for your support.

    May we know where can find more information about OTP24-31 are permanently write locked on devices without secure-boot option in the reference manual?

    PatrickFAnswer
    Technical Moderator
    June 27, 2022

    Hi @mikefae​ 

    See note 3 of Table 17 in RM0436 Rev.6

    In addition to Reference Manuel, the datasheet ordering information will tell you which device has secure-boot option (here STM32MP15xD or F could fit your needs).

    Regards,