Skip to main content
Visitor II
January 4, 2021
Solved

stm32mp1 watchdog command line test

  • January 4, 2021
  • 3 replies
  • 1193 views

Hi All,

i am getting watchdog Device or resource busy in stm32mp1

root@mp1som:~# dmesg | grep watchdog

[   2.108020] iwdg 5a002000.watchdog: unable to set timeout value, using default

[   3.642347] iwdg 5a002000.watchdog: timeout skrinked to 1

[   3.647585] systemd[1]: Hardware watchdog 'STM32 Independent Watchdog', version 0

[   3.654887] systemd[1]: Set hardware watchdog to 30s.

root@mp1som:~# echo V > /dev/watchdog

-sh: can't create /dev/watchdog: Device or resource busy

root@mp1som:~#

    This topic has been closed for replies.
    Best answer by Ara.1

    its working used following command

    wdctl

    3 replies

    Super User
    January 4, 2021

    How did you build your image? What version? Changes / additions? What mp1som?

    Ara.1Author
    Visitor II
    January 4, 2021

    Its customized image built using yocto, following distro is the details

    NOTE: Resolving any missing task queue dependencies

    Build Configuration:

    BB_VERSION          = "1.42.0"

    BUILD_SYS           = "x86_64-linux"

    NATIVELSBSTRING     = "universal"

    TARGET_SYS          = "arm-openstlinux_weston-linux-gnueabi"

    MACHINE             = "stm32mp1som"

    DISTRO              = "openstlinux-weston"

    DISTRO_VERSION      = "2.7-snapshot-20210104"

    TUNE_FEATURES       = "arm vfp cortexa7 neon vfpv4 thumb callconvention-hard"

    TARGET_FPU          = "hard"

    DISTRO_CODENAME     = "warrior"

    GCCVERSION          = "8.%"

    PREFERRED_PROVIDER_virtual/kernel = "linux-mp1som"

    Technical Moderator
    January 5, 2021

    Hi @Ara.1​ ,

    Looks like you are using a custom environment ( warrior + basic boot chain from V1.2 ecosystem) on a custom design based on SOM.

    I'm afraid this is too much custom to be efficiently supported in this community.

    I you confirm you are using a part from SOM maker integrating STM32MP1, please be aware that the SOM maker supposed to be your favorite support contact.

    If not please give more details in order we can provide relevant support.

    Olivier

    Ara.1AuthorAnswer
    Visitor II
    January 5, 2021

    its working used following command

    wdctl