STM32MP135 ADC buffer enable fails
Hi, I am encountering some issues while trying to configure the ADC DMA Buffer on the STM32MP135 board , when I execute the following:
echo 1000 > /sys/bus/iio/devices/iio:device1/buffer/length
echo 1 > /sys/bus/iio/devices/iio:device1/scan_elements/in_voltage0_en
echo 1 > /sys/bus/iio/devices/iio:device1/buffer/enable
I receive the following error after the third command:
sh: write error: Invalid argumet
But when reading the ADC's raw output directly via:
cat /sys/bus/iio/devices/iio:device1/in_voltage0_raw
I am able to obtain a normal reading, which suggests that the basic functionality of the ADC is intact.
Operating System: 5.15.24 #1 PREEMPT Sat Apr 13 15:11:38 CST 2024 armv7l GNU/Linux