Skip to main content
Explorer
August 7, 2024
Question

STM32MP135 Uboot libfdt fdt_check_header(): FDT_ERR_BADMAGIC

  • August 7, 2024
  • 2 replies
  • 2939 views

I'm trying to boot from SD-card and u-boot doesn't seem to find device tree. I have built my system with buildroot (bootlin st/2023.02.2) overriding the sources for tf-a, u-boot, op-tee and kernel, to be able to boot at least to u-boot (I did write another posts of my problems).

The files in SD-card

boot
├── extlinux
│ └── extlinux.conf
├── myb-stm32mp135x-512m.dtb
└── zImage

extlinux.conf

label myb-stm32mp135x-512m-buildroot
 kernel /boot/zImage
 devicetree /boot/myb-stm32mp135x-512m.dtb
 append root=/dev/mmcblk0p5 rootwait rw console=ttySTM0,115200

genimage

image sdcard.img {
	hdimage {
		partition-table-type = "gpt"
	}

	partition fsbl1 {
		image = "%ATFBIN%"
	}

	partition fsbl2 {
		image = "%ATFBIN%"
	}

	partition fip {
		image = "fip.bin"
	}

	partition u-boot-env {
		size = 2M
	}

	partition rootfs {
		image = "rootfs.ext4"
		bootable = "yes"
	}
}

So any ideas why it doesn't work?

    This topic has been closed for replies.

    2 replies

    jhiAuthor
    Explorer
    August 7, 2024

    I forgot to add the boot log

    Boot over mmc0!
    Saving Environment to MMC... Writing to redundant MMC(0)... OK
    switch to partitions #0, OK
    mmc0 is current device
    Scanning mmc 0:5...
    libfdt fdt_check_header(): FDT_ERR_BADMAGIC
    Scanning disk mmc@58005000.blk...
    Scanning disk mmc@58007000.blk...
    Found 16 disks
    No EFI system partition
    
    Error: eth2@5800e000 address not set.
    
    Error: eth1@5800a000 address not set.
    
    Error: eth2@5800e000 address not set.
    
    Error: eth1@5800a000 address not set.
    spi-nand: spi_nand MT29F2G01AB@0: unknown raw ID daf51a88
    Device spi-nand0 not found!
    ETZPC: 0x5a003000 node disabled, decprot 6=1
    FDT: cryp@54002000 node disabled for STM32MP135D Rev.Y
    BootOrder not defined
    EFI boot manager: Cannot load any image

     

     

    Technical Moderator
    September 20, 2024
    Graduate
    September 28, 2024

    Thanks a lot, Patrick. This worked for formatting the SD card. But I had some changed configuration, because of that It could not boot to linux. I changed my configuration, and from u-boot console I gave some boot command and after that, and it booted through Linux. Thanks again.

    Graduate
    September 19, 2024

    Hi, 

    were you able to solve your problem? I having similar issue.