Question
STM32MP135F-DK raspberry pi camera module v2.1
Hello,
I have STM32MP135F-DK board and raspberry pi camera module v2.1 but board does not see camera
I guess I have to modify stm32mp135f-dk.dtb file.
But how should I write settings like OV5640 or GC2145 in dtb file
like that
gc2145: gc2145@3c {
compatible = "galaxycore,gc2145";
reg = <0x3c>;
clocks = <&clk_ext_camera>;
IOVDD-supply = <&scmi_v3v3_sw>;
AVDD-supply = <&scmi_v3v3_sw>;
DVDD-supply = <&scmi_v3v3_sw>;
powerdown-gpios = <&mcp23017 3 (GPIO_ACTIVE_LOW | GPIO_PUSH_PULL)>;
reset-gpios = <&mcp23017 4 (GPIO_ACTIVE_LOW | GPIO_PUSH_PULL)>;
status = "okay";
port {
gc2145_ep: endpoint {
remote-endpoint = <&mipid02_0>;
clock-lanes = <0>;
data-lanes = <1 2>;
};
And after chaning that file should I do anything to take photo with raspberry pi camera module v2.1
And after chaning that file should I do anything to take photo with raspberry pi camera module v2.1