STM32MP135F: Unable to boot from SPI-NAND (GD5F4GM8UExxG)
Hello ST team,
I’m working on a custom board based on STM32MP135F SoC, with GigaDevice GD5F4GM8UExxG (512 MiB SPI-NAND) connected on SPI1 interface.
I’ve successfully integrated this NAND flash in U-Boot and Linux (Yocto build), but the board fails to boot directly from SPI-NAND. Please find the attached text file which is having the all changes.
When booting from SD card, I can probe, erase, and write to the SPI-NAND successfully — data can be read back and verified. please check below logs:
stm32mp13x:~# dmesg | grep spi
[ 0.708654] spi-nand spi0.0: GigaDevice SPI NAND was found.
[ 0.708678] spi-nand spi0.0: 512 MiB, block size: 128 KiB, page size: 2048, OOB size: 128
[ 0.708944] 9 fixed-partitions partitions found on MTD device spi-nand0
[ 0.708962] Creating 9 MTD partitions on "spi-nand0":
I can able to flash the image to spi-nand flash successfully after configuring in the uboot and tfa.
However, when I configure boot from QSPI-NAND, the boot ROM and TF-A logs indicate all blocks are bad. below is the log while booting from spi-nand
Exception mode=0x00000016 at: 0x2fff764c
NOTICE: CPU: STM32MP135D Rev.Y
NOTICE: Model: STMicroelectronics STM32MP135F-DK Discovery Board
INFO: Reset reason (0x34):
INFO: Pad Reset from NRST
INFO: FCONF: Reading TB_FW firmware configuration file from: 0x2ffe0000
INFO: FCONF: Reading firmware configuration information for: stm32mp_fuse
INFO: FCONF: Reading firmware configuration information for: stm32mp_io
INFO: Using SPI NAND
INFO: Instance 1
INFO: Boot used partition fsbl1
NOTICE: BL2: v2.10-stm32mp1-r2.0(debug):MYD-YF13X_2.10_V2.0.0_RC_20250926(e6a6fd49)
NOTICE: BL2: Built : 06:09:33, Aug 11 2025
WARNING: Block 8 is bad
WARNING: Block 9 is bad
WARNING: Block 10 is bad
WARNING: Block 11 is bad
WARNING: Block 12 is bad
WARNING: Block 13 is bad
WARNING: Block 14 is bad
.....
WARNING: Block 2044 is bad
WARNING: Block 2045 is bad
WARNING: Block 2046 is bad
WARNING: Block 2047 is bad
ERROR: mtd_add_extra_offset: Seek error -5
WARNING: Failed to load image id id=12 (-5)
WARNING: loading of FWU-Metadata failed, using Bkup-FWU-Metadata
ASSERT: drivers/io/io_mtd.c:140
Exception mode=0x00000016 at: 0x2fff764c
Hardware setup
SoC: STM32MP135F
Flash: GigaDevice GD5F4GM8UExxG (512 MiB, 2048 B page, 128 KiB block)
Interface: SPI1 @ 66 MHz (tried also 20 MHz, 104 MHz)
Boot source: SPI-NAND
- kernel : 6.6
- uboot: v2023.10
Yocto UBI configuration (256 MiB → 512 MiB updated)
# for 512 MiB GD5F4GM8UExxG
MKUBIFS_ARGS_nand_2_128_512 = "--min-io-size 2048 --leb-size 126976 --max-leb-cnt 4096"
UBINIZE_ARGS_nand_2_128_512 = "--min-io-size 2048 --peb-size 128KiB"
EXTRA_UBIFS_SIZE_nand_2_128_512 = "2816"
Could you please advise on:
Whether GD5F4GM8UExxG is officially supported by STM32MP135 boot ROM / TF-A SPI-NAND driver?
If the bad block scan mechanism or ECC layout needs adaptation for this device?
Whether TF-A expects any specific page / block geometry alignment for the bootloader region (fsbl1, fip-a1, etc.)?
Logs and configurations can be provided in full if needed.
Thanks,
Ganesh K