STM32MP135f VBat Current Consumption
Hello,
We are trying to run Tamper block in VBat (Vsw) mode. When we powered off the device, Vbat pin consumes 3 - 5uA from the battery as specified in device user manual.
As we understood from the documentation, the source of Vsw domain (either Vbat or VDD) is switched automatically by internal switch harware, so zero power consumtion is expected from battery when VDD is on.
In our custom board, when the board is powerd-up, VDD is on, VBat pin's power consumtion from battery increases up to 50-60uA.
Any recomendation about hardware or software would be very helpfull.
-The PDRON pin is pulled-up to VDD on the schematics.
- Battery is CR1216 - 3V Lithium Manganese Dioxide
- Battery is connected to the Vbat pin directly, no serial diode,resistor, etc...
- Battery cahrging feature is not enabled form device tree.