STM32MP15, cannot reboot in secure mode (TZEN = 1)
Hi,
I work on a custom board using a DHCOR SoM with a STM32MP157C SoC. I setup the TF-A + OP-TEE boot chain for the secure boot and I managed to boot on the linux stm32 (v6.1). The board hangs at reboot :
[ 1480.467975] reboot: Restarting system
I/TC: Forced system reset
To reboot the board, the OP-TEE OS writes '1' in the RCC_MP_GRSTCSETR register bit 0. If TZEN = '1', this register can only be modified in secure mode. TZEN is set to '1' by writing a '1' in the RCC_TZCR register bit 0, which is done by the rcc driver if the 'compatible' property is set to "st,stm32mp1-rcc-secure" in the OP-TEE device tree. The RCC is switched in "secure mode", which is confirmed at boot :
D/TC:0 0 check_rcc_secure_configuration:347 RCC/PWR secure hardening: TZEN enable, MCKPROT enableFrom the documentation, chapter 10.4.14 RCC TrustZone function :
"The bit TZEN allows the RCC and the PWR to be switched in secure mode. The RCC_TZCR register is only accessible by a secure access. When TZEN = ‘1’, some RCC and PWR registers can only be modified using secure accesses. The reading of registers is always allowed."
The secure attribute of the RCC_MP_GRSTCSETR register is "S", which means from the table 74 :
"This register can only be written in secure mode when TZEN = ‘1’ or when TZEN AND MCKPROT = ‘1’."
What I understand is that by setting RCC in secure mode with TZEN = '1' write access requires to be in secure mode. But what is the "secure mode" here ? What did I miss in my configuration ?
Regards,
Pierre-Loup