STM32MP151x: can I left the VDD3V3_USBHS Pin unconnected?
Hello,
according to the STM32MP151A/D Datasheet (Table 13.) the voltage on VDD3V3_USBHS Pin can be 0 ... 3.6V when USBH not used.
But on the another page of the Datasheet there is this section:
"VDD3V3_USBHS and VDD3V3_USBFS are respectively the USB high-speed and full-speed PHY supply. Voltage range is 3.07 V to 3.6 V. VDD3V3_USBFS is used to supply OTG_VBUS and ID pins. So, VDD3V3_USBFS must be supplied as well when USB high- speed OTG device is used. If not used, must be connected to VDD."
The last sentence is the opposite of the data given in Table 13.
Now I dont know what I am allowed to do? I dont need USB on my board and I dont want to add circuitry that is mandatory according to datasheets requirement: "VDDA1V8_REG must be present before VDD3V3_USBHS".
Thanks for help.