STM32MP153/157 periphery
Hey,
As a hardware engineer, I worked for a long time with the M7 controller.
For a Specific Algorithm, It seems like I should use a stronger core then the M7 480Mhz, when the purpose is to Calculate in Real-time.
one of the options is to use the MP153/157 with 2 cores 800Mhz each, for Better performance.
in case that I would like to work Bare metal- without operating system like Linux, and the entire purpose of the MPU is to calculate and send the data in serial communication, what is the minimum periphery the MPU Demands?
external DRAM is necessary ?
in simple words, can I just “supply�? the component?
what are the Consequences in using MPU Vs MCU, except from Power Consumption?
Best regards
peleg