STM32MP157 A7 and M4 communication
Hi,
I'am also using STM32MP157C-DK2 to communicate between the A7 and the M4 using the Virtual Uart (OPENAMP and IPCC).
I was trying to use STM32MXCube to configure the peripherals but the STM32MP157C-DK2 board is not available instead CubeMX has STM32MP157D DK1.
If I create a project in MXCube with MCU selector instead of Board selector it doesn't allow me to activate OpenAMP.
As both boards have similar hardware but different MCUs - CAC3 and DAC1 respectively can I still run MXCube project created by selection of 157D-DK1 board and run it on 157C-DK2 board.
Thanks in advance!
Mansi Patwari