Question
STM32MP157 on custom board: Start / Stop M4 FW via remote proc (stm32_rproc). Set BOOT_MCU bit
HOLD_BOOT: After an power-on reset the BOOT_MCU is '0' and we can set the
bit to '1', after an MCU reset (MCU_RST) the M4 FW start (CRun). All is fine.
But after that we can't reset the BOOT_MCU bit back to '0'. The BOOT_MCU bit
remains on '1' and we can't reach the HOLD_BOOT state again.
Is there any ideas why the BOOT_MCU bit remains on '1' ?!