STM32MP157 SDcard level shifter
Hi guys,
The schematics for STM32MP15x-EVAL board (MB1263) uses a level shifter for SDcard from NXP (IP4856CX25) that is now obsolete.
I found 2 close alternatives:
- ST6G3244MEBJR from ST, with one pin only (C4) different from IP4856
- TXS0206YFPR from TI, with 5 pins less then IP4856
Questions:
- Is it possible to use the ST6G3244 from ST replacing the IP4856CX25 from NXP? If so, is it a direct replacement (with pin C4 of STG3244 tied to GND)?
- I noticed that the NXP part has a wider host side voltage range up to 3V3 than the ST part. I don't have the MB1263 board here to measure, so I need to know what is the Voh of the SDcard lines in STM32MP157 in MB1263. Can anyone help me on this?
- Is it possible to use the TXS0206 from Texas which have a wider host side voltage range compatible with 3V3?
- Is there any other alternative to replace the IP4856CX25 from NXP?
Thank you guys in advance for any light on this topic.