Question
STM32MP157 Slave ADC can not get correct value.
Dear all,
I have a question about ADC.
When i used adc in dual regular simultaneous mode, master adc can get correct value, but slave adc can not.
Does anyone have some idea?
These are my ADC 1 and 2 configuration.
In my understanding adcData_DMA = ADC_CDR so adcData_DMA bits[31:16] = ADC2 Data. Is it right?

uint32_t adcData_DMA[5];
if (HAL_ADCEx_MultiModeStart_DMA(&hadc1,(uint32_t*)adcData_DMA, 5) != HAL_OK)
{
Error_Handler();
}ADC1

ADC2

Thanks.
Best Regards.