Skip to main content
Visitor II
May 15, 2025
Question

STM32MP157 USB enumeration question

  • May 15, 2025
  • 0 replies
  • 338 views

Hello, I would like to ask a question about the U-Boot USB enumeration of STM32MP157:
Using a custom board with the STM32MP157 (FUSB302MPX), openSTlinux6.6,:

Problem description:
Through "STM32_Programmer_CLI -c port=usb1 -d ../../FIP_artifacts/arm-trusted-firmware/tf-a-stm32mp157d-develop_mp157-mx-optee-programmer-usb.stm32 0x1 -s 0x1 -d ../../FIP_artifacts/fip/fip-stm32mp157d-develop_mp157-mx-optee-programmer-usb.bin 0x3 -s 0x3"
Write to the board memory, PC side
"Error: Unable to reconnect the target device: time out expired, Error: Start operation failed"

SullyNiu_0-1747302584625.png

 

On the board: Repeat log "dwc2_ep0_setup: bRequestType = 0x80(IN), bRequest = 0x6 wLength = 0xff, wValue = 0x302, wIndex= 0x409"

SullyNiu_1-1747302596632.png

Attached is the device tree and uart log.

    This topic has been closed for replies.