STM32MP157A-DK1 Enabling and reading STGEN.
Hi, I am working with STM32MP157A-DK1 board with Yocto build system.
I am trying to build synchronised system, that means I want to synchronise both CortexA7 and CortexM4. Basically I want to have the same time at both of them. I want to use STGEN for that, read it's counter on both A7 and M4 and share the values to calculate difference.
And here is my question, how can I enable STGEN in my own linux image (I am not using OpenSt distribution right now). My image is basing on core image minimal.
When I try to read STGENR registers provided in RM0436 with that piece of code (it is executed by M4):
#include "stgen_read.h"
#include "openamp.h"
#define STGENR_BASE_ADDR 0x5A005000UL
#define STGENR_CNTCVL_OFFSET 0x000
#define STGENR_CNTCVU_OFFSET 0x004
#define STGENR_CNTCVL_REG (*(volatile uint32_t *) (STGENR_BASE_ADDR + STGENR_CNTCVL_OFFSET))
#define STGENR_CNTCVU_REG (*(volatile uint32_t *) (STGENR_BASE_ADDR + STGENR_CNTCVU_OFFSET))
#Debug purpose
extern struct rpmsg_endpoint ept;
uint64_t stgen_get_counter() {
uint32_t low, high, high_comp;
do {
high = STGENR_CNTCVU_REG;
low = STGENR_CNTCVL_REG;
high_comp = STGENR_CNTCVU_REG;
} while (high != high_comp);
//temporary debug purpose
if (low == 0 || high == 0)
{
stgen_packet packet;
packet.type = 0xBB; #This means error packet
packet.data = 1;
rpmsg_trysend(&ept, &packet, sizeof(packet));
}
// end of debug
return ((uint64_t)high << 32) | low;
}I am always getting 0, basically this debug part is always executing.
I was trying to change STGEN access mode from secure to non-secure mode in ETZPC properties, in tf-a device tree, but at startup system is always in PANIC like here:

I also tried to add my own stgen node in kernel device tree but it didn't work. I will be grateful for any help and advice:).
Thank you in advance, please let me know if there is something that I can provide to make problem more clear.