STM32MP157A-DK1 StLink LED is always red
Hi,
When I power on my STM32MP157A-DK1 board, ST-LINK LED (LD4) is always red. On my Linux system when I connect the board through ST-LINK micro usb port (CN11), it is only detected as 'STM32 Virtual ComPort', and not detected as StLink device. And when I boot Linux, no activity on STM32 Virtual ComPort (/dev/ttyACM0).
It seems that there is an issue with on-board StLink.
Do you think this is a firmware issue that can be fixed or a hw issue?
Thanks,
Fatih