Question
STM32MP157C-DK2 board boot at panic mode
I flashed the board with dd command and tried either flashing whole SD card with the .raw image and each partition separately as well, it came up at panic mode. The image is en.FLASH-stm32mp1-openstlinux-5-10-dunfell-mp1-21-11-17_tar_v3.1.0. Does anyone have same problem?
root@stm32mp1:~# PANIC at PC : 0x2fff1f4b
Exception mode=0x00000016 at: 0x2fff1f4b