STM32MP157C-DK2 LCD SPI works with V4.1.0 DevPackage but not with V5.0.0
Hello, I've just migrated from V4.1.0 dev package to V5.0.0 and the LCD SPI ilitek 9486 does not work anymore.
Configuration: STM32MP157A-DK1 with 3.5 LCD SPI touchscreen. Starter Package loaded with stm32mp157c-dk2 config. Linux kernel recompiled with ili9486 module and uploaded. Device tree file "stm32mp157c-dk2.dts" modified with spi5 added and display and uploaded.
Please, how can I do to recover the LCD SPI that worked on previsous dev package?