Skip to main content
Visitor II
June 11, 2020
Question

STM32MP157C DSI for a 4 lane LCD (1280*800) PIXELS

  • June 11, 2020
  • 2 replies
  • 823 views

Hi:

I have a MIPI LCD ,the driver IC is S6D7AA0X04,the LCD brief shows that the data lane is 4,and the pixels is (1280x800) less than 1366*768,if LCD data lane is configurable,Can I drive it with the STM32MP157C?

thanks�?​

    This topic has been closed for replies.

    2 replies

    Technical Moderator
    June 11, 2020

    Hello,

    It should work, with checking on your LCD that it should be set to use 2 data lanes and could support a bandwidth of 1Gbit/s per lane (required to support 1280x800 24bits 60fps).

    Graduate II
    June 23, 2022

    Hello Patrick,

    I have the same question for an MIPI LCD, 4 lanes with the MP1

    it seems the LCD cannot be configured to 2 lanes with any pins

    LCD chipset = HX8282-A/C / HX8696-A01

    Resolution of 1024x600 16.7M and support colors

    Tlpxm and Tlpxd are 50nsec Min and 75nsec max.

    TTA-SUREs = 2xTlpxd

    TTA-GETD = 5xTlpxd

    TTA-GOD=4xTlpxd

    How to check from the chipset or LCD datasheet it can support the timing ?