stm32mp157c rpmsg comminucation problem
Hello,
I am working stm32mp157c. It has two processor (A7 and M4). They can communicate with each other over virt uart(rpmsg). When I want to send a message to a7 over m4, if the message is filled with constant data, everything is ok. If the message is filled with sequential data, the data cannot be fully transmitted. For example,
while(1)
{
OPENAMP_check_for_message();
uint8_t buffer[496] = { 0 };
for(uint16_t i = 0; i < sizeof(buffer); i++)
buffer[i] = 48;
VIRT_UART_Transmit(&huart0, buffer, sizeof(buffer));
HAL_Delay(1000);
}
In the above case everything is ok. But the following situation
while(1)
{
OPENAMP_check_for_message();
uint8_t buffer[496] = { 0 };
for(uint16_t i = 0; i < sizeof(buffer); i++)
buffer[i] = i;
VIRT_UART_Transmit(&huart0, buffer, sizeof(buffer));
HAL_Delay(1000);
}
It can only receive 251 of 496 bytes of data. IPCC clock speed is 210MHz.
What could be the problem?