STM32MP157D-DK1 missing RAM
Hello, I'm currently working with a STM32MP157D-DK1 Development Board with 4GB DDR3L. I populated the board with a prebuild openstlinux 6.1 build like discribed in a guide in the ST wiki.
When checking the total memory i unfortunatly only get 407MB that are used.
root@stm32mp1:~# free --mega
total used free shared buff/cache available
Mem: 407 138 152 13 140 269
Swap: 0 0 0
Is there a way to use the complete 4GB of RAM?
Kind regards,
Markus