STM32MP157F-DK, Run the SDK installation Error and Try to run python with Linux or flash it
I'd try to follow a step of Installing the SDK in Ubuntu (which is on Raspberry pi 4 Model B 4GB using 26GB SD card)
in step 4 Run the SDK installation script
I get an Error
Error: incompatible SDK installer! your host is aarch64 and this SDK was built for x86_64 hosts.
What does it mean and how can I fix it
The main goal of this project is to try to run python (with the library) on STM32MP157F-DK, I have two ideas
1. Follow the step and put it with .py instead of .c (no idea with install a library)
2. Install Linux in STM32MP157F-DK and run python on it (need some guild also)
So here I have 3 question
Thank STM for letting me ask a question here.