STM32MP157FAD schematic design
hi
I am working on a project using stm32mp157fad.
For the project created using stm32cubemx and stm32cubeide, I created a custom image by referring to the site below and uploaded it to the sd card using the dd command.
But openstlinux is not booting up so I want to check if there is a problem with the schematic.
1.Create an OpenSTLinux image
https://wiki.st.com/stm32mpu/wiki/How_to_create_your_own_machine
2.dd command
https://wiki.st.com/stm32mpu/wiki/How_to_populate_the_SD_card_with_dd_command
First of all, I would appreciate it if you could tell me if the circuit diagram is written correctly.
1.power circuit diagram
2.SD Card Used Pin
Second, I would like to know if the Boot-related program is entered in the ROM when the STM32MP1 series is shipped from the factory.
thank you