Question
STM32MP157x: Secure Boot authentication failed
hello I have build tf-a and u-boot and signed them as specified in the st wiki documentation:
But I get the following error when booting up:
NOTICE: CPU: STM32MP157FAC Rev.Z
NOTICE: Model: STMicroelectronics STM32MP157F-DK2 Discovery Board
NOTICE: Board: MB1272 Var4.0 Rev.C-02
NOTICE: Bootrom authentication failed
NOTICE: BL2: v2.6-stm32mp1-r1.0(release):v2.6-stm32mp-r1-3-gdbfd293df-dirty
NOTICE: BL2: Built : 13:17:15, Aug 5 2022
NOTICE: ROTPK is not deployed on platform. Skipping ROTPK verification.
NOTICE: ROTPK is not deployed on platform. Skipping ROTPK verification.
NOTICE: BL2: Booting BL32
NOTICE: SP_MIN: v2.6-stm32mp1-r1.0(release):v2.6-stm32mp-r1-3-gdbfd293df-dirty
NOTICE: SP_MIN: Built : 13:17:16, Aug 5 2022Note: I didn't deploy the publicKeysHashes.bin on my board since I'm using test keys (I's one time operation non revesible)
Is it required publicKeysHashes deployemnt required ?