STM32MP2: Modifying and using CubeMX Device Tree
Hey,,
I'm working on an STM32MP2 project and need help with Yocto. I generated a device tree with CubeMX and want to modify it so that I can activate the ums 0 mmc 1 command in the U-Boot terminal with the USB configured for 3.x speeds instead of the 2.0 basic configuration, then build a Yocto image (e.g., st-core-weston). Where do I place the DTS files, and how do I integrate them into the Yocto build?
Any tips or guides would be great!
Thanks!