Question
STM32MP2 performance - usable as basic notebook computer?
I'm very proud of STM32MP1 and I want to continue to learn more about the STM32MP products.
So, I'm planning to create another single board computer such as the open source project STM32-Computer. My next project will be STM64-Computer, which will use STM32MP257.
I have some questions that are refering to the STM32MP2 series.
- Can I surf on Youtube with that?
- Can I stream with that?
- Can I use regular programs such as Libre Office, Putty, Java, VS Code on that?
- Are there any limitations?
- How powerfull is the GPU? E.g can it do facial recognition?
- Is the setup, configuration, hard ware etc. almost the same as STM32MP1? I mean, if I have made a single board computer with STM32MP151, then a STM32MP257 will be exactly the same, just another more expensive and power full processor?
- Why is STM32MP257 so difficult to get? I can only see DigiKey have some few in stock.
- Is it possible to route the conductors on the PCB with 4 layers PCB, or do I need 6 layers or more for the STM32MP257? I know the getting started manual shows 6 layers. So I assume that 4 layers has been tested? The getting started manual for STM32MP1 shows 4 and 6 layers as an example and I have routed STM32-Computer with 4 layers. It works like a charm. Will it do the same for STM32MP257?
- Does a STM32MP2 really suit me as a personal computer?
- Where can I purchase STM32MP251? I don't need CAN or 3 different Ethernet. Only one.
Thank you!