STM32MP257F-DK CM33 peripheral initialization crashes A35
I generated the M33 code using CubeIDE by following the lab manual.
During the driver initializations:
MX_ADC1_Init();
MX_I2C1_Init();
MX_ICACHE_Init();
MX_RTC_Init();
The A35 halts CPU1 and resets after sometime.
E/TC:0 stm32_iac_itr:192 IAC exceptions [159:128]: 0x10000000
E/TC:0 stm32_iac_itr:197 IAC exception ID: 156
E/TC:0 Panic at /usr/src/debug/optee-os-stm32mp/4.0.0-stm32mp-r1/core/drivers/firewall/stm32_iac.c:212 <stm32_iac_itr>
E/TC:0 TEE load address @ 0x82000000
E/TC:0 Call stack:
E/TC:0 0x82007ed8
E/TC:0 0x82041b44
E/TC:0 0x8202c2c0
E/TC:0 0x8203f678
E/TC:0 0x82013cf4
E/TC:0 0x820017dc
I/TC: Halting CPU 1
Unfortunately I failed to create astable functional M33 for my MPU project yet. Are there no proper manual of code generation and configuration?