stm32mp257f-ev1 USB_DRD (CN15) configuration
Hello,
I notice that on stm32mp257f-ev1 board the USB_DRD port (CN15) is active only if USBPD_DRPSI_CM33_NonSecure_stripped.elf firmware is running. I need to run a different firmware on M33 while using the USB_DRD port. Searching in board's DT I found the following part:
&mlahb {
intc_rpmsg: interrupt-controller@1 {
compatible = "rpmsg,intc";
reg = <1 0>;
#interrupt-cells = <1>;
interrupt-controller;
status = "okay";
};
i2c_rpmsg: i2c@2 {
compatible = "rpmsg,i2c-controller";
reg = <2 0>;
rpmsg,dev-id = "rpmsg_i2c";
#address-cells = <1>;
#size-cells = <0>;
status = "okay";
typec@35 {
compatible = "st,stm32mp25-typec";
reg = <0x35>;
interrupts-extended = <&intc_rpmsg 0>;
status = "okay";
connector {
compatible = "usb-c-connector";
label = "USB-C";
port {
typec_ep: endpoint {
remote-endpoint = <&dwc3_ep>;
};
};
};
};
};
};So I'm thinking the point is that the typec@35 node is activated only when i2c_rpmesg is created running USBPD_DRPSI_CM33_NonSecure_stripped.elf. Is it possible to change this configuration?
Regards
Marco.