STM32NP157D Discovery Kit Getting Started: Kernel rebuild example hangs: ERROR: reserving fdt memory region failed (addr=d4000000 size=4000000) Any ideas?
I am evaluating the STM32NP157D Discovery Kit.
In the Getting Started Section I have successfully done the gtk_hello_world step.
The next step successfully rebuilds the kernel. After pushing it on the board I do the reboot and get the following Error message during booting:
# Booting kernel from Legacy Image at c2000000 ...
Image Name: Linux-5.10.61
Created: 2022-01-23 13:24:54 UTC
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 7465256 Bytes = 7.1 MiB
Load Address: c2000040
Entry Point: c2000040
Verifying Checksum ... OK
## Flattened Device Tree blob at c4000000
Booting using the fdt blob at 0xc4000000
XIP Kernel Image
ERROR: reserving fdt memory region failed (addr=d4000000 size=4000000)
Using Device Tree in place at c4000000, end c401efa2
Starting kernel ...
Now the system hangs.....