Support for 4 chips, 8bit ddr3 either 512m*8 or 1G*8?
Hey All,
So I know it's mentioned in the data sheet that the stm32mp1xx MPU's only support 16/32 bit DDR ram, and that it also mentions the limit of 1GByte total ram, but I just wanted to confirm this isn't possible and specifically why as I cannot find out much about what is the limiting factor here.
For example this IC:
Alternatively, could I push it up to 2GBytes by adding an additional MPU with its on 1GB of ram whilst also pushing it up as a quad core system?
And if so, what the best communication method would be between them.
Thanks in advance for any help!